FB#.MECHTYPE

Description

Sets whether the feedback is a rotary (0) or linear (1) encoder. If rotary, FB#.ENCLINES is the encoder resolution, and if linear, FB#.LINEPITCH.

Depending on the configuration and feedback type, this parameter is read only or read write. If used as a commutation feedback source for an axis (AXIS#.IL.FBSOURCE) this value matches AXIS#.MOTOR.TYPE for the corresponding axis. Otherwise, the value matches the feedback memory setting if available. Only if not assigned as an axis commutation source or unavailable through feedback memory will this value be settable by the user.

Context

See Feedback # View.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write or Read Only depending on configuration and feedback type

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable

FB1.MECHTYPE

3500h

0bh

Unsigned8

-

-

Read/Write

No

FB2.MECHTYPE

3501h

0bh

Unsigned8

-

-

Read/Write

No

FB3.MECHTYPE

3502h

0bh

Unsigned8

-

-

Read/Write

No

FB4.MECHTYPE

3503h

0bh

Unsigned8

-

-

Read/Write

No

FB5.MECHTYPE

3504h

0bh

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

FB1.MECHTYPE

30360

7698

Unsigned8

Read/Write

-

FB2.MECHTYPE

30361

7699

Unsigned8

Read/Write

-

FB3.MECHTYPE

30362

769A

Unsigned8

Read/Write

-

FB4.MECHTYPE

30363

769B

Unsigned8

Read/Write

-

FB5.MECHTYPE

30364

769C

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

FB1.MECHTYPE

30360

Unsigned8

Read/Write

-

FB2.MECHTYPE

30361

Unsigned8

Read/Write

-

FB3.MECHTYPE

30362

Unsigned8

Read/Write

-

FB4.MECHTYPE

30363

Unsigned8

Read/Write

-

FB5.MECHTYPE

30364

Unsigned8

Read/Write

-